This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM1808的转换延迟是多少

Other Parts Discussed in Thread: PCM1808, PCM1840

PCM1808从模拟信号输入到I2S信号输出的延迟时间是多少,或者怎样计算出来?我想选一个低延迟的音频ADC是否还有别的更好推荐,谢谢。

  • 您好,
    从数据手册18页7.4.2 Clock-Halt Power-Down and Reset Function描述来看,延迟应该是1024 SCKI+8960/fS,如果执行淡入操作需要48/fin或48/fS的额外时间。
    低延迟的音频ADC我再找一下。
  • 好的谢谢,我们准备用48KHz的采样速率,两路line in输入的音频ADC,帮忙看有没有转换速率比较快的音频adc,谢谢。

  • 非常抱歉,我上面回复的是复位后启动的延迟时间。经和同事确认后,稳态运行条件下的信号延迟主要由抽取滤波器决定,为17.4/fs。如果使用48kHz的采样率,所以延迟大约为362us。如果比较大,你可以考虑使用PCM1840,这是最近发布的一个更高性能的硬件控制ADC。这款ADC可以选择低延迟滤波器,延迟为7.7/fs,在48kHz的采样率下约为160us。