做好的板子,在输出同轴时,经常听到声音卡顿一下。时间间隔不固定,有时候三五分钟,有时候七八分钟。后来测量同轴输出的波形,感觉有点不对,麻烦TI的专家帮忙看看,原理图参考的也是官方原理图,没有变化。附图是原理图和在输出20Hz(前端调到20KHz波形也是这样)音频的情况下的波形。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
做好的板子,在输出同轴时,经常听到声音卡顿一下。时间间隔不固定,有时候三五分钟,有时候七八分钟。后来测量同轴输出的波形,感觉有点不对,麻烦TI的专家帮忙看看,原理图参考的也是官方原理图,没有变化。附图是原理图和在输出20Hz(前端调到20KHz波形也是这样)音频的情况下的波形。
我后端接的是DIR9001,这个IC输入前面有缓冲电路,你是担心因为RCA旁边接的那个75R的匹配电阻导致PCM2707C驱动不够吗?我的探头有10倍衰减,如果看图中的幅图,要乘以10,幅度应该够了。看波形,我感觉波形不太对,请看波形图,一个周期中,一共有三个波形的占空比不对(绿色箭头),而且是17个方波为一个循环,并且每次循环的占空比还有点不同(图中红色箭头)。我测量另一个其他方案的板子,他们输出的是16个方波为一个循环,其中有一个占空比稍有不同。另一个板子的最终输出还有个150R上拉和150R下拉的分压,最终经电容耦合输出在75R负载下,只有±0.4V的波形。PCM2707在输出75R的电阻后,比他这个波形还高。PCM2707C不需要软件控制吧,应该全硬件就可以输出吧。
今天有测试发现,这个波形的区别是不是因为采样率是44.1K和48K的区别?顺便再问一下,如果担心是后端DIR9001接收端的75R电阻导致驱动能力不足,可不可以增大这个电阻或者取消这个电阻?
昨天晚上去掉75R的电阻测试,还是会频偏,正常声音是有,间隔几分钟就会DIR9001就提示超出范围。
陈工:
现在把75R的负载去掉,用DIR9001输入的电路应该不存在驱动能力的问题了吧。数据传输还是经常出现错误,只是一瞬间,就类似那一瞬间DIR9001无法锁频一样,之后马上就正常了,后面还是每隔一段时间就出现一次。这个目前还有什么办法验证是哪里问题呢?