TPA3118和TPA3116的响应频率

 TPA3118和TPA3116的响应频率是多少?是否需要设置?比如我要用TPA3118做低音芯片的话最低频率可以响应到多少?

  • 您好,

    可以参考TPA3118数据手册图12. Gain/Phase(BTL)vs Frequency幅频特性曲线,最低到20Hz。
    一般音频芯片频率响应范围都是人耳可以听到的声音频率20HZ~20kHz之间。

    若该回复解决了您的问题,请点击“确认此为答案”,谢谢。

  • 回复 Amy Luo:

    比如这张表,假设我的增益是32dB,然后我用的input capacitance是1uf的话,是不是音频输入那端的信号一些低频会被砍掉,也就是 大概低于100Hz的音频都不会进入芯片中。

  • 回复 user5896736:

    您看数据手册举得这个例“If a flat bass response is required down to 20 Hz the recommended cut-off frequency is a tenth of that,2 Hz.表2 lists the recommended ac-couplings capacitors for each gain step.If a -3 dB is accepted at 20 Hz 10 times lower capacitors can used – for example, a 1 μF can be used”
    频响曲线有个平坦响应区域 flat response 和-3dB处,响应曲线是个斜坡,不是垂直上去的,所以说不能说低于100Hz的音频都不会进入,可以说低于100HZ的音频幅值有一定程度的衰减。

    若该回复解决了您的问题,请点击“确认此为答案”,谢谢。