This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3118D2音频功放的应用

Other Parts Discussed in Thread: TPA3118D2

Hi Ti工程师,

我司项目需求一颗音频功放,目前选用的TPA3118D2

附件为TPA3118D2在本项目原理图设计,请帮忙检查电路设计、器件选型等正确性,谢谢X6_RK3399_AUDIO_SCH-20210227.pdf

  • 您好,TPA3118D2有demo板,可以直接参考EVM user's guide Page6-11,包含了原理图,layout以及BOM表,希望对您有所帮助:
    www.ti.com.cn/.../slou342a.pdf
  • 1、MODSEL规格书定义两种模式: (LOW = BD mode, HIGH = 1 SPW mode).这两种模式区别是什么?

        我这边参考其他项目,大部分用法都是直接接地

    2、PVCC供电规格书给的是4.5V~26V  8A自适应,本项目采用12V/16A开关电源供电是否OK?

    3、DEMO图纸电阻、电容封装用的都较大,至少0603,此部分选型是否需完全follow?

    4、Pin6-PLIMIT、Pin7-GVDD、Pin8-GAIN/SLV三个脚接法请重点帮忙确认下

  • 1. 您好,1 SPW mode和BD mode的两种调制方式不同,具体可以参考FIgure32 和FIgure33.

    2. 12V在PVCC的电压范围内是可以的,但是输出功率是和供电电压有关系的,所以如果满足您的应用就行。

    3.是的,建议follow EVM user's guide中的电容规格,包括封装,比如0603或者0805,保证在一定的直流偏置电压下获得更好的容性。

    4.Pin6-PLIMIT、Pin7-GVDD、Pin8-GAIN/SLV接法可以参考datasheet中给出的电路, Plimit 接1uF到地,GAIN/SLV接分压电阻,R2 接GVDD, R1 接GND就好,R1和R2的阻值大小参考下面表格,根据不同Gain来取值。

  • 你好,

    1,本项目是基于RK3399,内置12V16A开关电源,BTL应用场景下,接两路4欧/65W音箱额定功率输出,PVCC供电怎么设计较合适?直接接12V开关电源,还是需要增加BOOST电路,采用24V供电?若需要BOOST电路,有低成本方案推荐嘛?

    2.PWM frequency建议设计为多少Hz?


  • Hi TI 工程师:
    1,本项目是基于RK3399,内置12V16A开关电源,BTL应用场景下,接两路4欧/65W音箱额定功率输出,PVCC供电怎么设计较合适?直接接12V开关电源,还是需要增加BOOST电路,采用24V供电?若需要BOOST电路,有低成本方案推荐嘛?

    2.PWM frequency建议设计为多少Hz?