Dear:
大家好,我在使用BQ25700模块的 OTG功能的时候发现OTG 输出电压比自己设置的偏小,例如设置了5v 实际输出4.2V左右,请问这大概是哪里的问题?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear:
大家好,我在使用BQ25700模块的 OTG功能的时候发现OTG 输出电压比自己设置的偏小,例如设置了5v 实际输出4.2V左右,请问这大概是哪里的问题?
谢谢!
你好,我这边的需求需要OTG 输出20V 5A的,这个要多大的电池电压才行?
Hi
要输出20V/5A,需要4节电池。
另外你用2节,设置输出5V是可以的,输出偏低,建议你确人一下相关配置。请问此时你带载是多少?