This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq25700芯片设置问题

您好!

      我们使用BQ25700作为充放电芯片,应用场合为AC输入电压12V,电池为2接电池8.4V,

测试过程中发现不对的地方如下:

      (1)、当没有接电池直接AC时,12V电源适配器输入,但是经过BQ25700后输出电压默认为6V,开机之后为上升至设置的充电电压8.6V。

     (2)、在开机过程中,负载不足2A,但是BQ25700输出电压经常会掉落至5V左右。

     麻烦各位大侠帮忙看看。