This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq34z100G1 电池学习后,放电过程中电量突然跳到0%,reset后又恢复电量是为什么呢?

使用瑟福21000mah的12芯电池,bq34z100G1 电池学习生成固件后,用120A左右的电流放电过程中电量大概到40%几就突然跳到0%,reset后又恢复电量是为什么呢?(用70A左右电流放电比较久才会出现这个问题,但是现象一样)

我注意到remain capacity跳为0、full charge capacity变成很小的数值:我烧另一次学习的固件问题依旧存在,但烧了另一种型号电池学习的固件,发现没有这个问题,请问各位大神可能是哪个地方做错了?谢谢!

放电前:

放电后: