This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27542电量芯片连接通信时断时续

使用BQ27542作为电量芯片,EV2300通信盒通信,连接BQ Studio软件打开自动刷新,会发现主界面的状态位有时会发生变化,感觉很不稳定,如图。电路图是按照规格书设计的,SDA和SCL通信使用的是300R和150pF、1M接法,唯一改动是需要通信接口输出1.8V,稳压采的是芯片的2.5V引脚串了一个0.7V二极管管降压,再由10K上拉的,请问一下技术支持,这种情况是怎么回事啊??而且进入data memory 中读数据的时候有时会出现a read of data written failed comparison,这个是不是没进入到寄存器读不到数据啊,然后多read all几次就可以读出来了。