This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24078充电的电压与电流都不正常

Other Parts Discussed in Thread: BQ24078

在调试BQ24078电源芯片.电路是应用资料的经典应用电路的接法.SYSOFF(15PIN)接的是GND.CE(4PIN).TMR(14PIN)EN1(6PIN)这三个引脚都是接GND的.VSS(8PIN)接GND.TS(1PIN)接的10K电阻.LILM(12PIN)接1.2K电阻ISET(16PIN)接1.2K电阻.PGOOD与CHG灯的指示脚也是按照应用电路接的.接的电阻是1K的.(EN2引脚是接芯片OUT引脚的)

.在空载(未焊接电池)上电时.测量充电口(BAT)充电电压一直在0V~4.3V之间一直在跳动.PGOOD引脚接的LED灯常亮.CHG引脚接的LED灯在上电瞬间闪烁了0.5S就灭了.

在接电池充电时.测的充电口BAT充电电压为4.3V电流为250MA.这实际不符合.因为电池是没有(电池电压为3.7V).这时的PGOOD与CHG引脚的灯都是常亮的.

请问我这该如何调试?问题出在那了?

  • 搞错了.SYSOFF接的是GND
  • HI
    充电时恒流,测试时要接电池的。
    充电电压建议至少4.35V(测试时建议用5V):注意EN1/EN2的配置,不要将其接到OUT, 可以接到IN或者GND.
    The bq2407x utilizes the VIN-DPM mode for operation from current-limited USB ports. When EN1 and EN2 are
    configured for USB100 (EN2=0, EN1=0) or USB500 (EN2=0, EN1=1) modes, the input voltage is monitored. If
    VIN falls to VIN-DPM, the input current limit is reduced to prevent the input voltage from falling further.
  • 你好!!
    因为我这边需要1.3A~1.5A的充电电流。这边引脚(EN2=1,EN1=0.)LILM=1.2K电阻.ISET=680Ω电阻.测试时,充电时.测得电池两端电压就跳到了4.35V?(未充电时.电池两端电压为3.67V)这是什么问题导致它跳到了那么高电压?配置USB500 (EN2=0, EN1=1) modes时.充电时电池两端为3.88V.(未充电时.电池两端电压为3.67V).电池电压马上提高了0.2V.这时的电池电压每过1秒就上升0.001V的电压(测得充电电流为300MA).请问该如何解决这些问题?
  • 你好,请问问题解决了吗?我们也遇到了同样的问题