This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25606在锂电池过放情况下充电会烧毁

Other Parts Discussed in Thread: BQ25606

Dears,

    我们用BQ25606给锂电池充电,为了测试可靠性,客户将锂电池过放电到1V以下甚至0V,然后用BQ25606给该过放的锂电池充电,此时BQ25606会变热变烫,最终烧毁,请问该现象原因是什么?如果避免这种故障现象?谢谢。

  • 您在做可靠性测试之前,充电器是否能正常工作。锂电池过放到0V可能已经损坏,无法充进去。
  • Hi
    BQ25606充电本质上是类似LDO,SYS最低电压3.5V作为LDO的输入,LDO的输出给到电池,此时如果LDO启动,等同于将LDO输出短到GND,电流很大会烧掉的。
    但是芯片本身是有保护的,不应该出现这类情况,例如有最低电池电压检测, sys过流保护, 电池short检测,电池过放保护。
    所以实际你试验的现象不会出现。