This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq27520开发板温度测量不准确问题

目前使用bq27520的demo板,连接我们的正式电池进行温度校准的时候(demo板的TS连接电池的温度传感脚),
测量实际电池温度是30度,但bqstudio界面中显示的温度是56度,校准后温度没有变化,仍然是56度。
若把demo板的TS端悬空,校准后可以达到30度。
与FAE联系得知需要修改DATA FLASH中的ext a coef 1-5及ext b coef 1-4,使用新提供的参数测量偏差更大,实际29度但显示-424度。
我在原来缺省参数基础上只修改了ext b coef 4后,在29度时显示的温度是正常的,但不清楚温度变化后是否会有问题。
手册上说需要使用10K NTC 103AT类型热敏电阻,我们目前使用的热敏电阻是NCP15XH103F03RC,B-Constant在25-50度是3380K,不知与手册上要求的是否相
符?若不符合如何计算来修改参数?