請問,我要使用BQ25713來管理NiMH這類型的電池
以下有幾個問題:
1.我們需求是Wide input voltage range,5~9V
2.power path function(Vsys=3.4~4.2v),是否可以設定?
3.Termination function,如何設定?
4.需求是NiMH=3CEL,3.6V~4.35V,是否能符合?
如有真實案例也可以提供參考~!
謝謝!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
当充电温度低于0.5C时,一般只能使用安全定时器来终止镍氢电池。BQ25896可以做到这一点,但4.2V的默认VBATREG和2A充电电流将需要通过I2C改变。
当电池在>0.5C充电时,强烈建议使用非常精确的dV/dt或dTemp/dt终止方法来终止镍氢电池,这是BQ25896无法做到的,即使使用主机软件及其7位ADC也不行。需要一个由主机控制的更精确的ADC来决定何时终止。