This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27742 怎么enable HDQ?

Other Parts Discussed in Thread: EV2400, BQSTUDIO, BQ27742EVM

如题,看资料说TI提供工具,没找到是用什么啊,请问怎么enable HDQ?

  • 官方的EVM板,下载调试工具用的是EV2300或者EV2400。如果自己的板子的话,就不需要了。
  • 我有EV2400和官方的EVM板啊,用I2C通讯没有问题,但是想用HDQ单线通讯模式。请问明白我的问题了吗? HDQ要ENABLE才能用,但是没找到怎么enable。
  • 好吧,我理解错了,sorry。我看官方EV2400的文档说明如下:
    2.4 HDQ Interface (HDQ)
    This interface port is not currently supported.
    EV2300才是支持HDQ的。
  • 我拿另外电池实际测试过了,EV2400也是支持的。但是提供的EVM不能通讯。

    The fuel gauge is shipped in the I2C mode. TI provides tools to enable the HDQ peripheral.

  • 莫非官方的手册没更新吗?反正EV2400这么高大上的应用我个人玩不起,说不定新版本的EV2400支持HDQ了。
  • Send HDQ Screen
    To configure a bq27742 fuel gauge into HDQ mode, navigate to the Send HDQ screen. It is possible that
    all the screen options on the left are not visible depending on screen resolution. If needed scroll within the
    left menu to access the Send HDQ link. Click on the "Change comm to HDQ8" button while having the
    bq27742 fuel gauge connected to the EV2300 interface board via I2C. Clicking on the button causes a
    message to appear indicating that the process is not reversible and to confirm if the actions are desired.
    Also, it explains what to do once the HDQ mode has been activated.
    但是EV2400界面我找了好久没有找到啊。
  • 反正我看官方的手册,说EVM2300是可以的,EV2400暂时不可以,或者说你需要更新新的GUI界面了。
  •     继续问,请Ti的工程师能帮我解答下吗? 谢谢!

  • Unfortunately the bqstudio for the bq27742 does not have the one click button that puts the device into hdq. However, you can trick the system using bqstudio for another device. Here is how:
    -disconnect the gauge from the computer by disconnecting the usb cable to the computer
    -start bqstudio and select gauge, then select bq27541-g1.
    -now plug in the bq27742 gauge by connecting the usb cable back.
    -the bqstudio for the bq27541 will detect communication and you should be able to cllick the i2c to hdq button o n there and put the device into hdq mode.

  • 厉害,找到问题了,哈哈。等我有钱了,也要买个开发板玩。
  • 您好!我按您方法试了还是不行,点击 Refresh没有反应,如果执行SEALED则提示SBM Write Word: No acknowledge from device。
    用I2C通讯则没有问题。
    根据您的描述,用HDQ不需要什么特殊的工具来Enable了? 我用EV2400加我手上封装好的电池,同样操作HDQ通讯就没有问题。那是不是说明我买的BQ27742EVM有问题? HDQ的pull-up已经加了JUMP了。电池4V时,测试HDQ为2.5V,插上EV2400接口连接PC后测试有2.7V。EVM买了没多久,我可以把这个EVM寄给您帮我测试确认下吗?
    非常感谢您的帮助。
  • 您的评估板是在哪里买的?建议您联系购买商
  • 您好!

            是在mouser.cn上买的,照理说应该不会有问题啊。就是说EVM 应该是不需要做任何改动,I2C和HDQ都能用才正常对吧? 刚我看也有人在问这个HDQ问题啊。看资料HDQ通讯是需要某种工具来enable的啊,不是直接和I2C共用的吧?

            感谢您的帮助,谢谢!

  • 您好!
    麻烦您能不能帮我确认板的问题呢,我找代理,代理说找网上供应商买一样的,所以就在mouser上买了。如果能帮我确认问题,我再找你们买1PCS吧,时间耗不起啊。拜托了!