This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24610的终止充电电流+预充电电流+电池充电电压设定的疑问

Other Parts Discussed in Thread: BQ24610

TI工程师你们好!

BQ24610的“终止充电电流/预充电电流/电池充电电压设定”,有几点疑问现向你们确认一下:

1.充电满电条件:是充电电流<终止充电电流,24610判定充电完成,stat2亮灯

                           还是电池电压上升>设定的电池充电电压,24610判定充电完成,stat2亮灯

    “充电电流和电池电压”这两个条件:逻辑上是什么关系?(如果只有一个条件达到设定标准,24610会表现异常状态吗)

2. Iterm:是终止充电电流吗?

   ①24610手册第26页Ipre-charge= Iterm=0.3A(是说:预充电流和终止充电电流在电路上都可以通过VISET2设定为0.3A吗?)

   ②24610手册第16页Ipre-charge=VISET2/100XRSR(是说:预充电流和终止充电电流都是可以人为设定的吗?)

   ③24610手册第17页“The minimum precharge/termination current is clamped to be
around 125 mA with default 10-mΩ sensing resistor.”(这个禁止充电电流125mA又是从何而来?125mA是固定的吗?与②是否有矛盾之处)

盼回复,请尽量用明确易懂的语言描述,谢谢!

  • 1,是的,预充电流和终止充电电流在电路上都可以通过VISET2设定
    2, 预充电流和终止充电电流可以设置为您需要的值
    3, 如果用10mohm的sense电阻,能 设置的最小预充电流和终止充电电流是125mA,电流再小精度不准
  • 感谢回复!可我的问题还有部份没有解决:
    1.我按手册第26页Ipre-charge= Iterm=0.3A,在电池端串接电流表实测:为什么充电电流降到150mA还在充电?监测在接近125mA时完成充电。这是为什么(电路照抄手册26页电路)?
    2.充电电流的减小和VFB电压的上升:这两个条件24610取那个条件做为“充电完成”的判定标准?如果只有一个条件达到设定标准,24610会表现异常状态吗?
  • 1. 您测量一下150是ISET2 的电压是否正确。
    2. 两个条件同时满足,充电电压和电流都达到截止条件才能完成充电
  • 明白了,是我用错了电阻,R6我用成了5.1K,实测ISET2电压为0.16V,谢谢您的回复!