This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教一下BQ25703A初始化寄存器的时候需要进行哪些配置?

Other Parts Discussed in Thread: BQ25703A

我的运用场景是BQ25703A给电池充电,需要输出15V 2A,目前只是大概进行了调下:

1.配置0x01寄存器,关掉WATCHDOG Timer

2.配置0x02 0x03寄存器配置充电电流

3.配置0x04 0x05寄存器配置充电电压

4.检测0x21寄存器bit7,给应用提供接口查看电源是否有接入

以上是我的配置,请问我这个配置是否有问题?有没有漏什么配置?或者有什么安全隐患?电池充满电后芯片是否需要手动配置充电电流为0?