This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教:使用BQ34z100-G1做放电测试,大电流情况下SOC突变为0%

您好,如题所述,在大电流放电时BQ34的SOC会突变为0,每次测试都是放出10%左右的电量后突变为0,电量变为0之后,手动复位BQ34后能够恢复正常电量,或者静置一会也会自动恢复正常电量;

Chemical ID是对的,也做了充放电的学习过程,使用的.srec文件之前一直再使用,没有遇见过这个问题,现在重新做了BMS板,使用同一款电芯,在大电流放电测试中出现了这个问题。

放电过程中Log:

6560.DisChargeTest.log
Thu Feb 25 11:58:10 CST 2021

Device Name = bq34z100G1
Firmware Version = 0_16


Sample,DateTime,ElapsedTime,Control,CtrlStatus,StateofCharge,MaxError,RemCap,FullChgCap,Voltage,Current,AvgCurrent,Temperature,AverageTimeToEmpty,AverageTimeToFull,AvailableEnergy,AveragePower,InternalTemperature,CycleCnt,StateofHealth,ChargeVoltage,ChargeCurrent,PackConfig,Flags,Flags B,GridNumber,LearnedStatus,DoDatEOC,Qstart,TrueRC,TrueFCC,StateTime,DOD0PassedQ,DOD0Time,DOD0,QmaxDOD0,QmaxPassedQ,QmaxTime,LogRowTime(ms),LogStatus
1,2021-02-25 11:58:15,4.669,0x0016,0x0015,80,1,3257,4111,24750,0,0,27.9,65535,65535,2306,0,27.9,2,100,26100,2150,0x29D8,0x0100,0x2400,0,6,0,854,3257,4111,279,0,1,3168,0,0,1,975,SUCCESS
2,2021-02-25 11:58:19,8.665,0x0016,0x0015,80,1,3257,4111,24750,0,0,27.9,65535,65535,2306,0,27.9,2,100,26100,2150,0x29D8,0x0100,0x2400,0,6,0,854,3257,4111,283,0,1,3168,0,0,1,931,SUCCESS
3,2021-02-25 11:58:23,12.762,0x0016,0x0015,80,1,3257,4111,24750,0,0,27.9,65535,65535,2306,0,27.9,2,100,26100,2150,0x29D8,0x0100,0x2400,0,6,0,854,3257,4111,287,0,1,3168,0,0,1,1314,SUCCESS
4,2021-02-25 11:58:27,16.678,0x0016,0x0015,80,1,3257,4111,24750,0,0,27.9,65535,65535,2306,0,27.9,2,100,26100,2150,0x29D8,0x0100,0x2400,0,6,0,854,3257,4111,291,0,1,3168,0,0,1,1336,SUCCESS
5,2021-02-25 11:58:31,20.687,0x0016,0x0005,80,1,3257,4111,23520,-21237,-1410,27.9,138,65535,2304,-16650,27.9,2,100,26100,2150,0x29D8,0x0101,0x0400,2,6,0,854,3247,4107,0,6,1,3168,0,6,1,1324,SUCCESS
6,2021-02-25 11:58:35,24.682,0x0016,0x0005,79,1,3233,4111,23232,-21001,-6135,28.0,32,65535,2295,-16263,28.0,2,100,26100,2150,0x29D8,0x0101,0x0400,2,6,0,854,3223,4107,4,30,1,3168,0,30,1,1236,SUCCESS
7,2021-02-25 11:58:39,28.685,0x0016,0x0005,79,1,3210,4111,23076,-20855,-9684,28.2,20,65535,2286,-16042,28.3,2,100,26100,2150,0x29D8,0x0101,0x0400,2,6,0,854,3200,4107,8,53,1,3168,0,53,1,1308,SUCCESS
8,2021-02-25 11:58:43,32.684,0x0016,0x0005,78,1,3187,4111,22986,-20751,-12352,28.6,15,65535,2277,-15883,28.6,2,100,26100,2150,0x29D8,0x0101,0x0400,2,6,0,854,3177,4107,12,76,1,3168,0,76,1,1155,SUCCESS
9,2021-02-25 11:58:47,36.679,0x0016,0x0005,77,1,3164,4111,22890,-20665,-14357,29.1,13,65535,2268,-15755,29.1,2,100,26100,2150,0x29D8,0x0101,0x0400,2,6,0,854,3154,4107,16,99,1,3168,0,99,1,1216,SUCCESS
10,2021-02-25 11:58:51,40.680,0x0016,0x0005,77,1,3141,4111,22818,-20613,-15862,29.7,12,65535,2259,-15653,29.7,2,100,26100,2150,0x29D8,0x0101,0x0400,2,6,0,854,3131,4107,20,122,1,3168,0,122,1,1220,SUCCESS
11,2021-02-25 11:58:55,44.683,0x0016,0x0005,76,1,3118,4111,22752,-20538,-16990,30.3,11,65535,2251,-15568,30.3,2,100,26100,2150,0x29D8,0x0101,0x0400,3,6,0,854,3108,4107,24,145,1,3168,0,145,1,1264,SUCCESS
12,2021-02-25 11:58:59,48.681,0x0016,0x0005,76,1,3095,4111,22698,-20502,-17835,31.0,10,65535,2242,-15494,31.0,2,100,26100,2150,0x29D8,0x0101,0x0400,3,6,0,854,3085,4107,28,168,1,3168,0,168,1,1251,SUCCESS
13,2021-02-25 11:59:03,52.682,0x0016,0x0005,75,1,3072,4111,22656,-20456,-18466,31.6,10,65535,2233,-15433,31.6,2,100,26100,2150,0x29D8,0x0101,0x0400,3,6,0,854,3063,4107,32,190,1,3168,0,190,1,1217,SUCCESS
14,2021-02-25 11:59:07,56.681,0x0016,0x0005,75,1,3050,4111,22614,-20418,-18831,32.3,10,65535,2225,-15375,32.3,2,100,26100,2150,0x29D8,0x0101,0x0400,3,6,0,854,3040,4107,36,213,1,3168,0,213,1,1189,SUCCESS
15,2021-02-25 11:59:11,60.680,0x0016,0x0005,74,1,3027,4111,22578,-20381,-19207,32.7,9,65535,2216,-15329,32.9,2,100,26100,2150,0x29D8,0x0101,0x0400,3,6,0,854,3017,4107,40,236,1,3168,0,236,1,1281,SUCCESS
16,2021-02-25 11:59:15,64.683,0x0016,0x0005,74,1,3004,4111,22548,-20351,-19484,33.4,9,65535,2208,-15280,33.5,2,100,26100,2150,0x29D8,0x0101,0x0400,3,6,0,854,2995,4107,44,258,1,3168,0,258,1,1219,SUCCESS
17,2021-02-25 11:59:19,68.685,0x0016,0x0005,73,1,2982,4111,22512,-20320,-19688,34.2,9,65535,2199,-15234,34.2,2,100,26100,2150,0x29D8,0x0101,0x0400,3,6,0,854,2972,4107,48,281,1,3168,0,281,1,1245,SUCCESS
18,2021-02-25 11:59:23,72.686,0x0016,0x0005,72,1,2959,4111,22482,-20293,-19835,34.6,9,65535,2191,-15196,34.7,2,100,26100,2150,0x29D8,0x0101,0x0400,3,6,0,854,2950,4107,52,303,1,3168,0,303,1,1083,SUCCESS
19,2021-02-25 11:59:27,76.680,0x0016,0x0005,72,1,2937,4111,22458,-20266,-19941,35.2,9,65535,2182,-15162,35.3,2,100,26100,2150,0x29D8,0x0101,0x0400,3,6,0,854,2927,4107,56,326,1,3168,0,326,1,1263,SUCCESS
20,2021-02-25 11:59:31,80.685,0x0016,0x0005,71,1,2914,4111,22434,-20239,-20015,35.7,9,65535,2174,-15127,35.8,2,100,26100,2150,0x29D8,0x0101,0x0400,3,6,0,854,2905,4107,60,348,1,3168,0,348,1,1219,SUCCESS
21,2021-02-25 11:59:35,84.680,0x0016,0x0005,71,1,2892,4111,22410,-20216,-20065,36.2,9,65535,2167,-15094,36.4,2,100,26100,2150,0x29D8,0x0101,0x0400,3,6,0,854,2882,4107,64,371,1,3168,0,371,1,1249,SUCCESS
22,2021-02-25 11:59:39,88.681,0x0016,0x0005,70,1,2869,4111,22386,-20193,-20098,36.8,9,65535,2157,-15060,36.9,2,100,26100,2150,0x29D8,0x0101,0x0400,3,6,0,854,2860,4107,68,393,1,3168,0,393,1,1275,SUCCESS
23,2021-02-25 11:59:43,92.682,0x0016,0x0005,70,1,2847,4111,22368,-20170,-20117,37.3,8,65535,2151,-15032,37.5,2,100,26100,2150,0x29D8,0x0101,0x0400,3,6,0,854,2837,4107,72,416,1,3168,0,416,1,1196,SUCCESS
24,2021-02-25 11:59:47,96.684,0x0016,0x0005,69,1,2824,4111,22344,-20151,-20127,37.9,8,65535,2142,-15008,38.0,2,100,26100,2150,0x29D8,0x0101,0x0400,3,6,0,854,0,1292,76,438,1,3168,0,438,1,1197,SUCCESS
25,2021-02-25 11:59:51,100.681,0x0016,0x0005,0,1,0,1292,22326,-20128,-20129,38.3,0,65535,0,-14979,38.4,2,100,26100,2150,0x29D8,0x0107,0x0400,3,6,0,854,-22,1292,80,460,1,3168,0,460,1,1278,SUCCESS
26,2021-02-25 11:59:55,104.683,0x0016,0x0005,0,1,0,1292,22302,-20109,-20126,38.7,0,65535,0,-14949,38.8,2,100,26100,2150,0x29D8,0x0107,0x0400,3,6,0,854,-45,1292,84,483,1,3168,0,483,1,1266,SUCCESS
27,2021-02-25 11:59:59,108.683,0x0016,0x0005,0,1,0,1292,22284,-20090,-20119,39.1,0,65535,0,-14923,39.2,2,100,26100,2150,0x29D8,0x0107,0x0400,3,6,0,854,-67,1292,88,505,1,3168,0,505,1,1195,SUCCESS
28,2021-02-25 12:00:03,112.682,0x0016,0x0005,0,1,0,1292,22266,-20069,-20108,39.5,0,65535,0,-14895,39.7,2,100,26100,2150,0x29D8,0x0107,0x0400,3,6,0,854,-89,1292,92,527,1,3168,0,527,1,1173,SUCCESS
29,2021-02-25 12:00:07,116.683,0x0016,0x0005,0,1,0,1292,22248,-20049,-20096,40.0,0,65535,0,-14868,40.1,2,100,26100,2150,0x29D8,0x0107,0x0400,3,6,0,854,-112,1292,96,550,1,3168,0,550,1,1276,SUCCESS
30,2021-02-25 12:00:11,120.681,0x0016,0x0005,0,1,0,1292,22230,-20030,-20082,40.4,0,65535,0,-14842,40.4,2,100,26100,2150,0x29D8,0x0107,0x0400,3,6,0,854,-134,1292,100,572,1,3168,0,572,1,1220,SUCCESS
31,2021-02-25 12:00:15,124.902,0x0016,0x0005,0,1,0,1292,22206,-20009,-20066,40.7,0,65535,0,-14809,40.8,2,100,26100,2150,0x29D8,0x0107,0x0400,3,6,0,854,-156,1292,104,594,1,3168,0,594,1,1322,SUCCESS
32,2021-02-25 12:00:23,132.886,0x0016,0x0005,0,1,0,1292,22176,-19973,-20033,41.3,0,65535,0,-14759,41.3,2,100,26100,2150,0x29D8,0x0107,0x0400,4,6,0,854,-201,1292,112,639,1,3168,0,639,1,1337,SUCCESS
33,2021-02-25 12:00:28,137.311,0x0016,0x0005,0,1,0,1292,22152,-19950,-20012,41.6,0,65535,0,-14731,41.7,2,100,26100,2150,0x29D8,0x0107,0x0400,4,6,0,854,-223,1292,116,661,1,3168,0,661,1,1207,SUCCESS
34,2021-02-25 12:00:31,140.681,0x0016,0x0005,0,1,0,1292,22140,-19936,-19999,41.9,0,65535,0,-14713,42.0,2,100,26100,2150,0x29D8,0x0107,0x0400,4,6,0,854,-245,1292,120,683,1,3168,0,683,1,1348,SUCCESS
35,2021-02-25 12:00:35,144.808,0x0016,0x0005,0,1,0,1292,22122,-19919,-19981,42.2,0,65535,0,-14688,42.2,2,100,26100,2150,0x29D8,0x0107,0x0400,4,6,0,854,-267,1292,124,705,1,3168,0,705,1,1414,SUCCESS
36,2021-02-25 12:00:39,148.701,0x0016,0x0005,0,1,0,1292,22104,-19902,-19964,42.4,0,65535,0,-14664,42.5,2,100,26100,2150,0x29D8,0x0107,0x0400,4,6,0,854,-284,1292,127,722,1,3168,0,722,1,919,SUCCESS
37,2021-02-25 12:00:43,152.701,0x0016,0x0005,0,1,0,1292,22086,-19885,-19946,42.7,0,65535,0,-14639,42.8,2,100,26100,2150,0x29D8,0x0107,0x0400,4,6,0,854,-306,1292,131,744,1,3168,0,744,1,970,SUCCESS

gg文件:

7282.gg.txt
* Texas Instruments Data Flash File,,,,
* File created Thu Feb 25 11:55:17 2021,,,,
*,,,,
* Device Number 100,,,,
* Firmware Version 0.16,,,,
* Build Number not available,,,,
* Order Number not available,,,,
*,,,,
* bqz Device Number 100,,,,
* bqz Firmware Version 0.16,,,,
* bqz Build Number 17,,,,
*,,,,
* Field Order: Class name, Subclass name, Parameter name, Parameter Value, Display Units
Configuration,Safety,OT Chg,55,1degC
Configuration,Safety,OT Chg Time,2,Seconds
Configuration,Safety,OT Chg Recovery,50,1degC
Configuration,Safety,OT Dsg,60,1degC
Configuration,Safety,OT Dsg Time,2,Seconds
Configuration,Safety,OT Dsg Recovery,55,1degC
Configuration,Charge Inhibit Cfg,Chg Inhibit Temp Low,0,1degC
Configuration,Charge Inhibit Cfg,Chg Inhibit Temp High,45,1degC
Configuration,Charge Inhibit Cfg,Temp Hys,5,1degC
Configuration,Charge,Suspend Low Temp,-5,1degC
Configuration,Charge,Suspend High Temp,55,1degC
Configuration,Charge,Pb Temp Comp,24.96,%
Configuration,Charge,Pb Reduction Rate,10,%
Configuration,Charge Termination,Taper Current,25,mAmp
Configuration,Charge Termination,Min Taper Capacity,7,mAmpHr
Configuration,Charge Termination,Cell Taper Voltage,100,mVolt
Configuration,Charge Termination,Current Taper Window,40,Seconds
Configuration,Charge Termination,TCA Set %,99,Percent
Configuration,Charge Termination,TCA Clear %,95,Percent
Configuration,Charge Termination,FC Set %,100,Percent
Configuration,Charge Termination,FC Clear %,98,Percent
Configuration,Charge Termination,DODatEOC Delta T,10,1degC
Configuration,Charge Termination,NiMH Delta Temp,3,1degC
Configuration,Charge Termination,NiMH Delta Temp Time,180,Seconds
Configuration,Charge Termination,NiMH Hold Off  Time,100,Seconds
Configuration,Charge Termination,NiMH Hold Off Current,240,mAmp
Configuration,Charge Termination,NiMH Hold Off  Temp,25,1degC
Configuration,Charge Termination,NiMH Cell Negative Delta Volt,17,mVolt
Configuration,Charge Termination,NiMH Cell Negative Delta Time,16,Seconds
Configuration,Charge Termination,NiMH Cell Neg Delta Qual Volt,4200,mVolt
Configuration,Data,Manuf  Date,2019/7/10,Day + Mo*32 + (Yr -1980)*256
Configuration,Data,Ser. Num.,106,hex
Configuration,Data,Cycle Count,2,Count
Configuration,Data,CC Threshold,3000,mAmpHr
Configuration,Data,Max Error Limit,100,%
Configuration,Data,Design Capacity,4300,MilliAmpHour
Configuration,Data,Design Energy,16280,MilliWattHour
Configuration,Data,SOH Load I,-400,MilliAmp
Configuration,Data,Cell Charge Voltage T1-T2,4350,mV
Configuration,Data,Cell Charge Voltage T2-T3,4350,mV
Configuration,Data,Cell Charge Voltage T3-T4,4350,mV
Configuration,Data,Charge Current T1-T2,10,Percent
Configuration,Data,Charge Current  T2-T3,50,Percent
Configuration,Data,Charge Current  T3-T4,30,Percent
Configuration,Data,JEITA T1,0,degC
Configuration,Data,JEITA T2,10,degC
Configuration,Data,JEITA T3,45,degC
Configuration,Data,JEITA T4,55,degC
Configuration,Data,Design Energy Scale,5,Number
Configuration,Data,Device Name,BMS-HV,-
Configuration,Data,Manufacturer Name,ZT,-
Configuration,Data,Device Chemistry,LION,-
Configuration,Discharge,SOC1 Set Threshold,150,mAh
Configuration,Discharge,SOC1 Clear Threshold,175,mAh
Configuration,Discharge,SOCF Set Threshold,75,mAh
Configuration,Discharge,SOCF Clear Threshold,100,mAh
Configuration,Discharge,Cell BL Set Volt Threshold,3600,mVolt
Configuration,Discharge,Cell BL Set Volt Time,2,Seconds
Configuration,Discharge,Cell BL Clear Volt Threshold,3700,mVolt
Configuration,Discharge,Cell BH Set Volt Threshold,4380,mVolt
Configuration,Discharge,Cell BH Volt Time,2,Seconds
Configuration,Discharge,Cell BH  Clear Volt Threshold,4350,mVolt
Configuration,Discharge,Cycle Delta,0.05,%
Configuration,Manufacturer Data,Pack Lot Code,0,hex
Configuration,Manufacturer Data,PCB Lot Code,311,hex
Configuration,Manufacturer Data,Firmware Version,106,hex
Configuration,Manufacturer Data,Hardware Revision,3,hex
Configuration,Manufacturer Data,Cell Revision,0,hex
Configuration,Manufacturer Data,DF Config Version,0,hex
Configuration,Integrity Data,Static Chem DF Checksum,7c70,Number
Configuration,Lifetime Data,Lifetime Max Temp,42.2,1degC
Configuration,Lifetime Data,Lifetime Min Temp,8.7,1degC
Configuration,Lifetime Data,Lifetime Max Chg Current,3206,mAmp
Configuration,Lifetime Data,Lifetime Max Dsg Current,-21676,mA
Configuration,Lifetime Data,Lifetime Max Pack Voltage,1307,20mV
Configuration,Lifetime Data,Lifetime Min Pack Voltage,175,20mV
Configuration,Lifetime Temp Samples,LT Flash Cnt,24,Count
Configuration,Registers,Pack Configuration,29d8,flags
Configuration,Registers,Pack Configuration B,af,flags
Configuration,Registers,Pack Configuration C,37,flags
Configuration,Registers,LED_Comm Configuration,43,flags
Configuration,Registers,Alert Configuration,1,flags
Configuration,Registers,Number of series cell,6,num
Configuration,Lifetime Resolution,LT Temp Res,1,1degC
Configuration,Lifetime Resolution,LT Cur Res,100,mA
Configuration,Lifetime Resolution,LT V Res,1,20mV
Configuration,Lifetime Resolution,LT Update Time,60,Seconds
Configuration,LED Display,LED Hold Time,4,Num
Configuration,Power,Flash Update OK Cell Volt,2700,mVolt
Configuration,Power,Sleep Current,10,mAmp
Configuration,Power,FS Wait,0,Seconds
System Data,Manufacturer Info,Block A 0,0,hex
System Data,Manufacturer Info,Block A 1,0,hex
System Data,Manufacturer Info,Block A 2,0,hex
System Data,Manufacturer Info,Block A 3,0,hex
System Data,Manufacturer Info,Block A 4,0,hex
System Data,Manufacturer Info,Block A 5,0,hex
System Data,Manufacturer Info,Block A 6,0,hex
System Data,Manufacturer Info,Block A 7,0,hex
System Data,Manufacturer Info,Block A 8,0,hex
System Data,Manufacturer Info,Block A 9,0,hex
System Data,Manufacturer Info,Block A 10,0,hex
System Data,Manufacturer Info,Block A 11,0,hex
System Data,Manufacturer Info,Block A 12,0,hex
System Data,Manufacturer Info,Block A 13,0,hex
System Data,Manufacturer Info,Block A 14,0,hex
System Data,Manufacturer Info,Block A 15,0,hex
System Data,Manufacturer Info,Block A 16,0,hex
System Data,Manufacturer Info,Block A 17,0,hex
System Data,Manufacturer Info,Block A 18,0,hex
System Data,Manufacturer Info,Block A 19,0,hex
System Data,Manufacturer Info,Block A 20,0,hex
System Data,Manufacturer Info,Block A 21,0,hex
System Data,Manufacturer Info,Block A 22,0,hex
System Data,Manufacturer Info,Block A 23,0,hex
System Data,Manufacturer Info,Block A 24,0,hex
System Data,Manufacturer Info,Block A 25,0,hex
System Data,Manufacturer Info,Block A 26,0,hex
System Data,Manufacturer Info,Block A 27,0,hex
System Data,Manufacturer Info,Block A 28,0,hex
System Data,Manufacturer Info,Block A 29,0,hex
System Data,Manufacturer Info,Block A 30,0,hex
System Data,Manufacturer Info,Block A 31,0,hex
Gas Gauging,IT Cfg,Load Select,1,Number
Gas Gauging,IT Cfg,Load Mode,0,Number
Gas Gauging,IT Cfg,Max Res Factor,50,num
Gas Gauging,IT Cfg,Min Res Factor,1,num
Gas Gauging,IT Cfg,Ra Filter,500,num
Gas Gauging,IT Cfg,Min PassedChg NiMH-LA 1st Qmax,50,%
Gas Gauging,IT Cfg,Maximum Qmax Change,100,%
Gas Gauging,IT Cfg,Cell Terminate Voltage,3000,mVolt
Gas Gauging,IT Cfg,Cell Term V Delta,200,mVolt
Gas Gauging,IT Cfg,ResRelax Time,500,Seconds
Gas Gauging,IT Cfg,User Rate-mA,0,MilliAmp
Gas Gauging,IT Cfg,User Rate-Pwr,0,mW/cW
Gas Gauging,IT Cfg,Reserve Cap-mAh,0,MilliAmpHour
Gas Gauging,IT Cfg,Reserve Energy,0,mWh/cWh
Gas Gauging,IT Cfg,Max Scale Back Grid,4,num
Gas Gauging,IT Cfg,Cell Min DeltaV,0,mVolt
Gas Gauging,IT Cfg,Ra Max Delta,15,%
Gas Gauging,IT Cfg,Design Resistance,62,mOhms
Gas Gauging,IT Cfg,Reference Grid,4,-
Gas Gauging,IT Cfg,Qmax Max Delta %,10,mAmpHour
Gas Gauging,IT Cfg,Max Res Scale,32000,Num
Gas Gauging,IT Cfg,Min Res Scale,1,Num
Gas Gauging,IT Cfg,Fast Scale Start SOC,10,%
Gas Gauging,IT Cfg,Charge Hys V Shift,40,mVolt
Gas Gauging,IT Cfg,Smooth Relax Time,1000,s
Gas Gauging,Current Thresholds,Dsg Current Threshold,20,mAmp
Gas Gauging,Current Thresholds,Chg Current Threshold,20,mAmp
Gas Gauging,Current Thresholds,Quit Current,10,mAmp
Gas Gauging,Current Thresholds,Dsg Relax Time,10,Seconds
Gas Gauging,Current Thresholds,Chg Relax Time,10,Seconds
Gas Gauging,Current Thresholds,Cell Max IR Correct,400,mV
Gas Gauging,State,Qmax Cell 0,4416,mAmpHr
Gas Gauging,State,Cycle Count,1,num
Gas Gauging,State,Update Status,6,num
Gas Gauging,State,Cell V at Chg Term,4350,mVolt
Gas Gauging,State,Avg I Last Run,-4251,mAmp
Gas Gauging,State,Avg P Last Run,-3098,MilliWattHour
Gas Gauging,State,Cell Delta Voltage,19,mVolt
Gas Gauging,State,T Rise,20,Num
Gas Gauging,State,T Time Constant,1000,Num
Ra Table,R_a0,R_a0 Flag,ff55,Hex
Ra Table,R_a0,R_a0 0,121,Num
Ra Table,R_a0,R_a0 1,86,Num
Ra Table,R_a0,R_a0 2,96,Num
Ra Table,R_a0,R_a0 3,106,Num
Ra Table,R_a0,R_a0 4,87,Num
Ra Table,R_a0,R_a0 5,89,Num
Ra Table,R_a0,R_a0 6,96,Num
Ra Table,R_a0,R_a0 7,91,Num
Ra Table,R_a0,R_a0 8,95,Num
Ra Table,R_a0,R_a0 9,98,Num
Ra Table,R_a0,R_a0 10,95,Num
Ra Table,R_a0,R_a0 11,115,Num
Ra Table,R_a0,R_a0 12,164,Num
Ra Table,R_a0,R_a0 13,254,Num
Ra Table,R_a0,R_a0 14,355,Num
Ra Table,R_a0x,R_a0x Flag,ffff,Hex
Ra Table,R_a0x,R_a0x 0,121,Num
Ra Table,R_a0x,R_a0x 1,86,Num
Ra Table,R_a0x,R_a0x 2,96,Num
Ra Table,R_a0x,R_a0x 3,106,Num
Ra Table,R_a0x,R_a0x 4,87,Num
Ra Table,R_a0x,R_a0x 5,89,Num
Ra Table,R_a0x,R_a0x 6,96,Num
Ra Table,R_a0x,R_a0x 7,91,Num
Ra Table,R_a0x,R_a0x 8,95,Num
Ra Table,R_a0x,R_a0x 9,98,Num
Ra Table,R_a0x,R_a0x 10,95,Num
Ra Table,R_a0x,R_a0x 11,115,Num
Ra Table,R_a0x,R_a0x 12,164,Num
Ra Table,R_a0x,R_a0x 13,254,Num
Ra Table,R_a0x,R_a0x 14,355,Num
Calibration,Data,CC Gain,2.486,mohm
Calibration,Data,CC Delta,2.482,mohm
Calibration,Data,CC Offset,-1461,num
Calibration,Data,Board Offset,-14,num
Calibration,Data,Int Temp Offset,-1.2,degC
Calibration,Data,Ext Temp Offset,0,degC
Calibration,Data,Voltage Divider,30189,mVolt
Calibration,Current,Deadband,10,mAmp
Security,Codes,Sealed to Unsealed,57784888,hex
Security,Codes,Unsealed to Full,ffffffff,hex
Security,Codes,Authen Key3,1234567,hex
Security,Codes,Authen Key2,89abcdef,hex
Security,Codes,Authen Key1,fedcba98,hex
Security,Codes,Authen Key0,76543210,hex