This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于BQ51013B与bq500211无线接收与发送电压不到5V

Other Parts Discussed in Thread: BQ51013B, BQ500211, BQ51013, BQ51013A

无线收发器设:接收端利用bq51013B参照bq51013xEVM-764 Evaluation Module (WCSP Package)》进行电路板设计;发送端利用的是bq500211,参照《bq500211EVM-045 bqTESLA Wireless Power TX EVM User's Guide》,设计完成的电路板。存在问题:空载时bq500211的输出电压在0到2伏之间跳动,发送端和接收端的板子上的灯均在闪动。接上10欧姆纯电阻负载测试,调节ILIM端的5kΩ的电位器,可以将输出电压升至4.5V(此时接收端的等保持持续亮的状态),但是继续增加电压时接收端电压却跳变为0了,出现了不稳。请问这个问题怎么解决?电压到不了5V?

想咨询下无线收发正常工作时可以以5V,200~400mA左右的电流进行持续的对外供电吗?谢谢!

  • 1.Bq51013B可以连续输出5v/1A的电流(注意散热方面的设计)。

    2、关于你所提的问题,建议你申请TI的EVM来分别你所设计的TX或RX进行测试,这样可以方便地定位究竟是你的TX,还 是RX有问题。

    3、对于TX,请问你提线圈和谐振电容是谁提供的,值是多少?

    4、对于RX,问题同#3。

  • 非常感谢Ken Zhang工程师的热心解答!关于线圈和电容:

    1..发送端采用的线圈是伍尔特的760308111,见:http://katalog.we-online.de/en/pbs/WE-WPCC#vs_ct:5

            谐振电容为100*4 nF的电容,按照《bq500211 Schematic and Materials Application Package》中给的值,从中发配的料;

    2.采用的接收线圈是伍尔特的760308201,见:http://katalog.we-online.de/en/pbs/WE-WPCC/760308201?sid=494e880055;

             采用的谐振电容是68、68、47nF,按照bq51013xEVM-764手册中给的值,从中发配的料;

            现在的问题是能够稳定的输出5V的电压了,但是现在的问题是带载能力不行,当负载(采用纯电阻负载测试)大于10欧姆时,输出电压能够较好的稳定在5V,当负载小于5欧姆后,电压就迅速下降,如当负载为5欧姆,电压下降到了3.21V左右,想请问一下:

    1.如何增强线圈的带载能力?

    2.bq500211和bq51013配合使用能够输出5W的功率吗?

    3.还有一个问题就是在HPA764 Schematic中的R17(30.9kΩ)好像去了对电路也没有多大影响(之前未焊接和焊接对比),是这样的吗?

    还有R15、D2、C20的作用是给en1、en2提供高电平吗?见附件中标明~~

    谢谢!

  • 1.如何增强线圈的带载能力?---->你可以参考“http://www.ti.com/analog/docs/litabsmultiplefilelist.tsp?literatureNumber=slyt479&docCategoryId=1&familyId=64"中应用文档,去设计接收端线圈。请确保你的线圈有能力输出5W(感量要够,谐振电容要对,磁芯不能饱和)。

    2.bq500211和bq51013配合使用能够输出5W的功率吗?----可以。

    3.还有一个问题就是在HPA764 Schematic中的R17(30.9kΩ)好像去了对电路也没有多大影响(之前未焊接和焊接对比),是这样的吗?----> R17在Bq51013B中对FOD调试有用。对BQ51013A,无用。

    还有R15、D2、C20的作用是给en1、en2提供高电平吗?见附件中标明~~   ----正确.

  • 您好,请问您是怎样解决不能稳定输出5V电压的问题的呢?

  • 请问:你是指什么情况下,输出不稳定?轻载时,重载时,还是动态载输出时?

  • 现在是这样的,我想用bq51013 来实现交流转直流,负载电阻在13欧左右,但是输出电压只有2.9V-3V,远远达不到5V

  • 你好,请问你问题原因事什么,最终怎么解决的,我现在做了个无线接收端的板子,输出电压只有1.2~1.3V,想请教下你