此电路用于给3节锂电池2A充电,输入15V,但充不进去。该电路,在不接电池时输出端不是该有12.6的电压吗?现在FB只有0.14V,BAT只有0.8V,为什么?经测,各个引脚电平也是正常的。ACDRV=21V, CMSRC=15V, VREF=3.3V, ISET=0.4V, ACSET=0.8V, AVCC=15V, OVSET=1.2V, TS=1.9V, REGN=6V, BATDRV=15V, SW=SRP=SRN=0.8V。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,TS脚需要接电池的NTC,如果不接,可以使用一个10K的电阻代替,并在TS和GND之间
可以测量一下system电压是否等于输入,谢谢。
您好,
如果系统直接从电池取电,可以不加。如果从VSYS取电,需要加MOS和驱动,为了降低电池到系统之间的压降。
请检查每个引脚的电压波形,看是否正常?
谢谢