This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI能量采集芯片bq25505、bq25504、bq25570输出电流是多少?

我希望通过外部的能量采集,供给100mA的无线装置,可否实现?

  • 这个问题需要仔细的评估各项参数,与能量源的特性直接相关,比如它在启动BQ芯片的条件下所能够提供的电流是多少?以太阳能采集板举列,板子的规格,日照的时间,采用的储能电池的大小,平均的负载和系统功耗,从而判断储能电池需要支撑的时间以及采集板规格是否合适。对于大多数能量采集的BQ芯片,是允许100mA负载的。

    以上谢谢!

  • 太阳能板供给电流是80mA,但是仿真显示IDIN_dc是0mA