This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50出现CTO和CFETF错误?

Other Parts Discussed in Thread: BQ40Z50-R1

客户寄回两个电池(2s2p的),cell 1和2电池电压读取为3.728V 和 3.727V。芯片是用的BQ40Z50-R1。

通过上位机读取状态为,如下图所示:

从上图中可以看到,充放电MOS管都关闭了,然后CTO(充电超时安全保护被触发)和CFETF(充电MOS管出现PF错误),实验证明,CTO触发后,充电器还接在电池上,但电流会降低到几乎为0,实际没有触发CFETF错误。百思不得其解,请TI工程师,有经验的前辈指点指点,谢谢!!!

 

  • 系统提示充电MOS失效,从而引起充电超时错误,请查看一下充电MOS硬件有没有问题,同时看一下电池在静置状态下,电流是否归0了。如果确认没有问题,可以考虑把PF关掉,或者是将BQ40Z50R1出厂时上锁,以免出现在使用过程中,数据出错的情况。