使用BQ76940+BQ78350做了一个BMS,由于系统的开机电流比较大,达到16A。
按照BQ78350的TRM,修改OCD threshold数值,改成 -30000mA。
实测的过程中,发现该值无效,开机后直接进入OCD保护模式
似乎系统的OCD threshold仍然是6000mA。
此外,系统运行起来以后,电流可能达到50A,如何设置OCD threshold数值呢?
根据TRM的描述,OCD threshold最多只能到-32000mA。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.