This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25713 NiMH

Other Parts Discussed in Thread: BQ25713, BQ25896

請問,我要使用BQ25713來管理NiMH這類型的電池

以下有幾個問題:
1.我們需求是Wide input voltage range,5~9V

2.power path function(Vsys=3.4~4.2v),是否可以設定?

3.Termination function,如何設定?

4.需求是NiMH=3CEL,3.6V~4.35V,是否能符合?

如有真實案例也可以提供參考~!

謝謝!!

  • 我看了,好像都沒有回答到我的問題,我再提一次
    1.Termination function,如何控制?
    2.因為我們使用的電壓,都是跟鋰電池1cell的電壓相同,我們是用3S的NiMH=4.35V,所以預設值是Li的值,我的理解應該是ok吧?
    3.power path function,因為我們的需求是,有Vin時,system的電壓由Vin供給,但是system的range是3.4~4.2v,如何設定?
    再麻煩回覆以上問題,謝謝你~!
  • 1.In regards to NiMH termination, the common techniques would be 1) delta temperature based, 2) delta voltage based, and 3) safety timer based. Again, refer to your NiMH battery specification.
    2. 是的,默认是锂电池的,设置CELL_BATPRES pin来设置您的NiMH
    3. System Voltage Regulation 范围是1.024V~19.2V,您可以通过寄存器设置REG0X0D/0C()
  • 容許我再問一個問題~

    我的條件如下:

    NiMH電池3串,3.6~4.35V電壓範圍

    我要管理上述的電池組,我可否用BQ25896?

    如你說的,NiMH電池的重點有3個,delta temperature,delta voltage,safety timer~

    上述三樣,BQ25896都可以達成,電池電壓也符合需求,我的理解應該是因為VBAT的電壓範圍限制,導致這顆BQ25896在官網上沒有描述可以用在NiMH

    可否幫忙確認這顆是否可以用在我的應用上面?

    謝謝你~!

  • 当充电温度低于0.5C时,一般只能使用安全定时器来终止镍氢电池。BQ25896可以做到这一点,但4.2V的默认VBATREG和2A充电电流将需要通过I2C改变。

    当电池在>0.5C充电时,强烈建议使用非常精确的dV/dt或dTemp/dt终止方法来终止镍氢电池,这是BQ25896无法做到的,即使使用主机软件及其7位ADC也不行。需要一个由主机控制的更精确的ADC来决定何时终止。