This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76925芯片使用问题--单体电压误差

Other Parts Discussed in Thread: BQ76925

你好,我在使用BQ76925该芯片时遇到如下问题:

     1.单体电压采样时,安装官方的DEMO每节电池采样间隔32ms,大部分没有问题,但部分芯片出现莫一节电芯电压偏低很多的情况,见如下图片,我尝试将间隔时间改为100m后,恢复正常,再次修改为32ms,仍然正常,请问这是什么问题,如果我的程序按照32ms设计如果出现如何处理,如果全部设计为100ms那么会不会有其他芯片还出现这样的问题?

     开始有问题的波形

 正常的波形

    2.电流采样在电流时,VIOUT引脚输出不是官方的2.0V,而是2.2V左右,我们按照2.2与2.0的比例进行电流校准,目前测试几PCS都比较准确,但这样是不是有依据,批量生产会不会出现其他问题?

      3.电芯采集电压矫正问题。官方推荐采用增益误差和偏移量误差来矫正采集到的单芯电压,但是我们矫正以后电压总有一节电芯电压不准确,误差在20%;而不使用增益误差和偏移量误差不矫正,可以将误差做到5%,但是还是无法达到官网10mV以内。这是什么原因呢?为啥不矫正比矫正的还要准确?

   以上三个问题,希望得到尽快回复!