请问DS90UB953和DS90UB954的组合,是否支持4M以上分辨率的摄像头?比如我们使用13M的sensor,进行全尺寸拍照或者1080P60fps视频传输?
另外DS90UB954是否支持两路1080P 60fps 的视频同时聚合复用接收?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问DS90UB953和DS90UB954的组合,是否支持4M以上分辨率的摄像头?比如我们使用13M的sensor,进行全尺寸拍照或者1080P60fps视频传输?
另外DS90UB954是否支持两路1080P 60fps 的视频同时聚合复用接收?
1)不支持4M以上分辨率哦:The DS90UB953-Q1 serializer represents the next generation in FPD-Link III serializers and is designed to support high-speed raw data sensors including 2MP imagers at 60-fps and as well as 4MP, 30-fps cameras, satellite RADAR, LIDAR, and Time-of-Flight (ToF) sensors
2)可以,通过配置寄存器0X0C来控制port 0 还是其中之一enable,还是二者均enable,或者二者均disable(在不用的前提下)。
这句话的意思是支持2MP60-fps和4MP30-fps和其它摄像头,并没有提到最大的分辨率,请再确认下,谢谢。
我理解是如果降低帧率,比如10fps,这时候带宽支持更高的分辨率。
能够支持多大分辨率,是由pixel clock决定的,高频模式,DS90UB953的像素时钟最大为100MHz。
比如1920*1080p@60Hz的分辨率,需要的像素时钟要为148.5MHz, 因此这个就不能够支持。
DS90UB953不是支持2M@60Hz吗?怎么1920*1080p@60Hz不支持?请问像素时钟是如何计算的?
Kailyn,您好!我们用953和954,目前自己设计的953板子和954和DSP设计在一块板子,954这端一直接收不到MIPI数据,走的是TP(双绞线传输模式),Sensor用的OV2740(2MP的sensor), 在953端可以检测到MIPI数据,但954端接收不到MIPI数据,I2C信号是通的。
从953端向954端发Pattern数据,4个Lane时,954端可以接收到数据,但换成2个Lane模式,954端接收不到MIPI数据。求助您帮忙,提供建议如何解决,我们3个星期都没找到原因~