This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2594EVM Reference Pro 不与电脑连接

Other Parts Discussed in Thread: LMX2594EVM, LMX2594, USB2ANY

你好,

LMX2594EVM Reference Pro 不与电脑连接,请问如何解决?

多谢!

王斌林

  • 您好,请参考user guide检查硬件的设置是否OK

    www.ti.com.cn/.../snau210.pdf

  • Reference Pro上的MSP 430的LED灯会亮吗?

  • 你好,

    按照user guide操作,测试环境及方法为:

    1,使用仪表:笔记本电脑,Agilent E4405B 频谱分析仪,40dB衰减器,直流电源。

    2,直流电源输出设置为3.3V,限流 450mA。

    3,使用方法:按照 LMX2594 EVM Instructions – 15-GHz Wideband
    Low Noise PLL With Integrated VCO User's Guide 连接电源,频谱仪,笔记本,EVM板。按照 User's Guide给不用的端口接50欧姆负载。

    4,测试步骤:连接好后,打开测试工具TICS Pro,打开电源 3.3V,待机时电流约为170mA,工作后电流约为390mA。频率、功率都可以调节。测试时频率设置为7GHz。

    5,故障现象:正在工作时,突然没有输出,测试工具显示USB无连接。

  • TI你好,

    因当前任务紧,没有太多时间等待最终解决方案。这个问题能否这样处理,

    1,先给我们换一块Reference Pro 板,让我们继续测试LMX2594EVM。把坏的Reference Pro 板寄给TI继续分析,寻找问题点。

    2,为解决此问题,我们在TI官网上研读了大量与Reference Pro、LMX2594EVM、TICS Pro、USB2ANY等相关文献。经我司分析,初步判断,Reference Pro板上的U1输出电压太低,约为0.7V(在Reference Pro板上的C3、C20上测试),导致U4(M430)不能正常工作,不能与电脑连接的故障。我司打算尽快自行修复Reference Pro板,只去掉U1,看看结果如何。