This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1148八通道数据采集问题

Other Parts Discussed in Thread: ADS1148, ADS1247

在使用ADS1148芯片进行八通道数据采集时遇到的现象,参考电压选择2.048V,AIN0-AIN3转换正常,但是AIN4-AIN7的AD转换值的参考电压好像是1.25V左右,而不是2.048V的参考电压,请问TI员工,这个问题是怎么回事?要怎么解决?

  • 使用的是内部参考吗?切换到AIN4-AIN7通道时,测得内部参考输出电压VREFOUT 为1.25V是吗?
  • VREFOUT用万用表测出的电压一直都是2.048V,但是AIN4-AIN7的实际输出ADC值不对,我实际测的AIN6电压为0.582V(理论转换AD值应该是9312),AIN7为0.442V(理论转换AD值应该是7072),,但是实际输出AD值AIN6是16572左右,AIN7是13320左右,这个实际AD值和参考电压是1.25V的时候理论计算输出很接近,所以不知道这是怎么回事。
  • 同样遇到这种问题, 用了3片采集,某一片AD值不正常跳变大
  • 现在用ADS1247,80sps采样率下,AD值变化有低14位;20sps采样率下,AD值变化低8位;这是24位AD,难道不能用80sps或者更高的采样率获得比较稳定的AD值吗?电路是AIN0是一个0~0.6V的直流信号,AIN1接地,用吉时利的7位半的万用表测量信号只有变化几uv,应该不会有低14位AD值变化。有没有高手指导下,为什么会这样?1k的sps采样率完全不能用