This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB914与DS90UB913 I2C通信问题

现通过914配置913:

1)直接读取914的0x00,返回0xC0。

2)   直接读取914的0x06,可自动获取913的地址0xB0。

3)   直接读取914的0x03,返回0xE9。

4)   直接读取914的0x21,返回0x17。

5)配置SER_Alias地址0x07,写入别名0xB2。

6)读取913器件(0xB2) 的0x00地址,无法获取。

7)测量lock脚,一直为低,测量I2C信号发现写0xB2后, ACK无响应。

这是什么问题导致这种情况?

(ds90ub914与DS90UB913分2块板,914工作电压在3.3V,913工作电压在1.8V,这是否存问题)