This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS8200-EP是否支持BT.1120输入、VGA输出?

Other Parts Discussed in Thread: THS8200-EP, THS8200

Dears,

烦请帮忙确定一下THS8200-EP是否支持BT.1120输入、VGA输出,多谢!

Thanks!

  • BT.1120 是20bit位宽4:2:2格式,内嵌同步信号。
    THS8200 的数字输入端包括BT.1120,所以是支持的,数据手册中有描述:
    THS8200 can accept a variety of digital input formats, in both 4:4:4 and 4:2:2 formats, over a 3×10-bit, 2×10-bit or 1×10-bit interface.
  • Dear Kailyn,

    感谢您的回复,
    除了THS8200以外,还有什么产品可以支持BT.1120输入、VGA输出吗?
    THS8200-EP和THS8200的区别是什么?为什么价格相差那么大?

    Thanks!
  • 视频DAC 系列的产品好像只有THS8200这款,并且已经处于NRND状态。
    和THS8200-EP的差异在于,EP指的是enhanced product,主要用于航空航天,高温度场合等的应用,满足一些行业标准。 请看下对EP的详细介绍:
    Enhanced Products are plastic packaged solutions that have been have been qualified and certified to the Aerospace Qualified Electronic Component (AQEC) Standard (ANSI/GEIA STD-0002-1). The AQEC Standard was jointly developed by the aerospace and semiconductor industries to define the minimum requirements for commercial-off-the-shelf (COTS) components used in military, avionic, aerospace, medical and other rugged operating environments where high-reliability and long service life are required.