This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求教18位以上ADC 用REF2025这种参考后,还需要在参考电压加buff再做低通滤波吗?

Other Parts Discussed in Thread: REF2025, OPA350

求教18位以上ADC 用REF2025这种参考后,还需要在参考电压加buff再做低通滤波吗? 我看到好多设计用了AZ431,然后加了OPA350做电压跟随器,然后OPA350输出做了低通滤波,求解这样设计原因。

  • 您好,首先OPA350的轨至轨输入输出,单位增益稳定,高速,低噪声的这些特点非常适合用于驱动ADC。

    您可以看下OPA350 在驱动ADC方面的介绍:
    OPA350 series operational amplifiers are optimized for driving medium speed (up to 500 kHz) sampling A/D converters, and also offer excellent performance for higher speed converters. The OPA350 series provides an effective means of buffering the input capacitance of the A/D and resulting charge injection while providing signal gain.