This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1220在连续转换模式下测试时出现死机

Other Parts Discussed in Thread: ADS1220

用ADS1220测试电压(感性负载电压)时,有时出现ADS1220停止转换,读取值一直为0的现象。如果重新对ADS1220发送复位命令和启动连续转换命令后,ADS1220 又重新工作,读取值又正常。我想问一下ADS1220 的模拟输入信号电压如果受到尖脉冲干扰,是否会死机?

  • 您好,
    感谢您对TI产品的关注!在异常时,您有测量DRDY信号有持续发出吗,您可以用示波器测量CS、SCLK、DOUT、DRDY信号吗,以检测进入死机时,这些信号是否发生了异常
  • 您好
    由于条件所限,无法用示波器观察测量CS、SCLK、DOUT、DRDY端的信号是否出现了异常,因为SPI通信线上只有一个ADS1220,所以CS是直接接地的,只能通过ADS1220的转换数据出现一直为0,类似停止转换时,然后重新对ADS1220发送复位命令和启动连续转换命令后,ADS1220 又重新工作,读取值又正常。来判断是ADS转换死机的问题。另外结合出现这种异常现象时,ADS1220 的输入模拟信号电压出现干扰的可能性非常大,因为测试的是感性负载的工作电压,测试过程中测试回路有时会出现电打火的现象,干扰是肯定存在的。现在就是想请教一下,ADS1220这个AD在测试这种感性负载的电压时,是否有出现死机的可能?那么可以采取哪些措施来克服?或者需要注意些什么?谢谢!