大家好!
我想选用ISO7721用于485隔离,遇到带你问题,请帮忙看看。
①看到PDF上描述IIH(High-level input current)最大到10uA,但是MCU SCI TX引脚输出一般是mA级的,所以是不是需要在输出脚串一个K级的电组来限流?
②我查阅了TI所有跟ISO7X21的参考设计原理图,其中没有任何一张原理串联了上面描述的限流电阻,为什么?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这个参数的意义是,当输入ISO77xx输入I/O是高电平,也就是上拉到VCC供电时,I/O的电流为10uA。即使你的MCU能够提供超过10uA,芯片本身只会需要10uA的电流。在正常情况下,相当于负载只有10uA,因为输入一般是比较器,输入阻抗比较高。
在实际中,可以在引脚上串电阻,主要是为了防止干扰的脉冲电流窜入芯片,实现保护的功能。