This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1247用1k采样率AD值波动很大

Other Parts Discussed in Thread: ADS1247

现在用ADS1247,80sps采样率下,AD值变化有低14位;20sps采样率下,AD值变化低8位;这是24位AD,难道 不能用80sps或者更高的采样率获得比较稳定的AD值吗?电路是AIN0是一个0~0.6V的直流信号,AIN1接地,用 吉时利的7位半的万用表测量信号只有变化几uv,应该不会有低14位AD值变化。 用8422的输出接到ADS1247的输入采样,这样接法测出来的AD值波动有14位,电源和输入信号都用高精度万用 表测试只有几uv的波动 8422输出阻抗应该比较低了,请教一下用过AD1247的大神们帮忙找找原因,非常感谢了!!!!

  • 我觉得与你的应用有关
    确实, ADC 通常较高的精度就需要较低的采样率, 不过原因来自于电路里的开关噪声, 引起电源纹波, 参考基准, 以及受限于信号源的阻抗.
    所以提高精度你要从多个方面下手
  • 经过测试ADS1247的供电2.5v,-2.5v,输入的信号接到AIN0,GND接到AIN1,相当于单端输入,这些信号测试都是在uv波动,最多就是10uv波动,但是获得的AD值波动有12位,都有1mv波动了,
    用的内部2.048v基准;
    AD8422的输出阻抗不高的,而且ADS1247的输入阻抗几百兆欧姆
    不知道到底哪里出了问题,麻烦大神帮忙看看。非常感谢了