This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC7725可否与DSP直接连接

Other Parts Discussed in Thread: DAC7725

我想使用DSP28335配合DAC7725进行DA输出。输出范围是0-10V。

数据表中,逻辑输入为0.8V为低,2.4V为高。当DSP的数据总线与DA的总线直接连接时,可以写入。但是同时提到,芯片可以返回DA通道的寄存器值,而逻辑输出在5v供电情况下,逻辑信号输出为0.4V为低,3.6V-VDD为高。这样是否会损坏DSP引脚。我是否可以直接将DA芯片的VDD使用3.3V供电,以消除对DSP的影响。