This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1278使用中经常烧坏1-2个通道

Other Parts Discussed in Thread: ADS1278, PGA281, OPA2227, REF5025

    大家好,我现在使用的ADS1278工作频率是10.24MHz,配置的采样频率的1KSPS,供电是+5VDC给了AVDD,+3.3VDC给了IOVDD,+1.8V给了DVDD,用示波器看上电顺序是:先有+5V,隔了1ms+3.3V开始达到要求,再隔大概1秒+1.8V才能达到要求,这就和芯片手册推荐的上电顺序完全相反,至于为什么这样做是因为,我的电路板是通过先有+5V然后再通过LDO产生了+3.3V,最后再通过+3.3V和LDO产生+1.8V,目前,我的ADS1278很容易损坏1-2个通道,经常是使用中通道1和通道2的AD结果变为负的最大值,芯片偶尔有发热的现象,但是在芯片不发热的时候也经常表现为前2个通道损坏,我想问专家们,是不是这个上电顺序导致的ADS1278频繁坏的原因?非常感谢您的解答。