This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

紧急!ADS8528 内部基准输出偏差较大

Other Parts Discussed in Thread: ADS8528

ADS8528使用硬件串行模式,使用内部基准,2VREF模式, REFIO引脚输出基准电压在+3.165到+3.182之间(测试三块相同的板子),通过FPGA经过ADS8528

的RESET引脚对ADS8528复位,同样REFIO输出电压在在+3.165到+3.182之间,和理论的2*2.5V(5V)输出基准偏差较大,麻烦帮我解答以下,谢谢!

  • 2VREF不是REFIO的输出电压,这个是AD输入的范围。REFIO的输出电压是VREF,范围为0.2VREF-VREF之间,可是你VREF选择2.5V的话,REFIO的输出值确实偏大了。
  • 您好,

    使用内部基准,默认值是2.5V,范围是2.496V~2.504V,REFIO输出电压在在+3.165到+3.182之间确实不应该,可以提供接线图和寄存器配置更多的信息吗,还有所使用芯片是从TI授权的代理商处购买的吗