大家好,我有一个ADS1220的问题请教。
我用ADS1220测量桥式传感器,测量正常没有问题。现在的问题是,我想用信号源输出一个10mV的信号,作为基准校准采集精度,
但是,这个信号源输出的10mV信号,接入ADS1220时,读取的AD值是一个变化的值,且无规律(信号源已经和ADS1220共地)。
我的疑问是,ADS1220设置为差分信号输入(支持伪差分),信号源输出的10mV信号与地之间,不是可以当做一个伪差分信号吗?
为什么采集不到正确的AD值?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好:
PGA enable Gain=128 ,我的接法是差分输入负端(引脚7)接GND,差分输入正端(引脚10)接信号源的正端(10mV信号)。信号源与ADS1220共地。
寄存器设置0x3E 0xC4 0x98 0x00。
关键问题,这种接法,测量桥式传感器正常。我现在想要用同样的方法,测量10mV的信号源,结果不正常。