This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1220上电之后DOUT脚始终是高电平

Other Parts Discussed in Thread: ADS1220

您好:

请教一下各位前辈,我是新手,使用F28M35设备上的SPI接口连接ADS1220,采集单端信号,DSP上一个SPI接口并联挂载了5个SPI设备,调试ADS1220时,将其他SPI设备片选拉高旁路。上电之后,ADS1220的DOUT脚为高电平,读0x00配置寄存器(发送0X20),DIN脚波形正常,但是DOUT脚持续高电平,是否是ADS1220芯片有问题?或者电路驱动能力不足?还是其他的一些问题,还请大家不吝赐教~

附件波形图中:

1通道为DIN,2通道为DOUT,3通道为SCLK

代码用的ADS1220官方代码。

  • 您好,
    感谢您对TI产品的关注!检查下通信电平是否不兼容?DSP上SPI接口工作电平是几伏的呢
  • 您好:
    谢谢您的回复!
    测试的这组ADS1220设备SPI电平是和DSP(F28M35x)引脚电平匹配的,都是3.3V。
    但是SPI并联的5组设备里还有一组ADS1220设备,供电为4.3V左右,当前的测试里没有被片选,应该是不影响吧。
    测试部分:
    先操作片选信号,对ADS1220发送一个字节0X06复位信号。然后延迟1s,保证复位初始化完成。然后读00寄存器值到BUFF变量,读到了0XFF,操作向00寄存器
    写config[0]=0x94,再次读00寄存器到read[0],还是0xFF。
    代码如下:
    SPI配置波特率1MHz,SpiaRegs.***.bit.CLKPOLARITY = 0;   SpiaRegs.***.bit.CLK_PHASE = 1;SpiaRegs.***.bit.*** = (8-1);
    while(1) { GpioDataRegs.GPBDAT.bit.GPIO59=0;//CS LOW DELAY_US(2); /* send the command byte */ ADS1220SendByte(0x06);//RESET CMD DELAY_US(500000); GpioDataRegs.GPBDAT.bit.GPIO59=1;//CS HIGH DELAY_US(500000); write[0]=ADS1220ReceiveByte();//KEEP FIFO EMPTY ADS1220ReadRegister(ADS1220_0_REGISTER, 0x01, &BUFF);//READ THE 0X00-REGISTER DELAY_US(20); /* write the register value containing the new value back to the ADS */ ADS1220WriteRegister(ADS1220_0_REGISTER, 0x01, &config[1]); read[1] = ADS1220ReceiveByte();//KEEP FIFO EMPTY read[2] = ADS1220ReceiveByte();//KEEP FIFO EMPTY DELAY_US(4); ADS1220ReadRegister(ADS1220_0_REGISTER, 0x01, &read[0]); DELAY_US(10); }

  • 您好,测试的这组ADS1220设备SPI电平是和DSP(F28M35x)引脚电平匹配的,都是3.3V。
    但是SPI并联的5组设备里还有一组ADS1220设备,供电为4.3V左右,当前的测试里没有被片选,应该是不影响吧。
    测试部分:先操作片选信号,对ADS1220发送一个字节0X06复位信号。然后延迟1s,保证复位初始化完成。然后读00寄存器值到BUFF变量,读到了0XFF,操作向00寄存器写config[0]=0x94,再次读00寄存器到read[0],还是0xFF。
    代码如下:SPI配置波特率1MHz,SpiaRegs.***.bit.CLKPOLARITY = 0; SpiaRegs.***.bit.CLK_PHASE = 1;SpiaRegs.***.bit.*** = (8-1);
  • 您可以实测一下ADS1220的CS的电平吗,以确认一下CS已被拉低