This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65HVD230的ESD保护二极管怎么选择

Other Parts Discussed in Thread: SN65HVD230

根据手册,SN65HVD230的CANH(CANL)到GND的最大电压在-4V -- 16V。而多数厂家生产的用于CAN-BUS的ESD保护二极管breakdown电压都在20多伏。很想用SN65HVD230这个芯片,能否帮助推荐保护用的TVS二极管?谢谢

  • 选取TVS时,至少选择TVS的stand-off voltage, Vwm要大于等于总线电压。比如CANH(CANL)到GND的最大电压在-4V -- 16V,那么TVS的Vwm>=16V.

    按照TVS的VI传输特性,breakdown电压还要大于Vwm,所以选择20多伏是可以的。 

  • 根据手册,-4V -- 16V是最大能承受的电压,到这个数值时已经会损坏芯片。如果我选择TVS的Vrwm(min)为24V, Vbr(max) 32V,那么16V-26V的电压加在总线上还是要损坏芯片的呀。请问TI有没有合适的TVS呢,结电容<30pf,sot23封装的就行。

  • 楼下说的有道理,同关注该问题
  • 你好,

    首先必须明确TVS管作为保护器件,用来防止静电或者浪涌击穿保护电路。和通常的稳压管的功能有一定的差别。
    其次,CANH(CANL)到GND的最大电压在-4V -- 16V指的是总线到地的共模电压的范围,CAN总线最后传输的信号状态与CANH和CANL之间的差分信号的范围有关。因此在选择TVS管注意VRWM大于正常线路的供电电压,并且保证Vc小于芯片规定的16V即可。
    请问选择sot23封装的原因是什么啊?如果并不是必须的可以到以下连接选择TI的TVS管,封装比通用的TVS管小。
    www.ti.com/.../description