This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FPGA+DS90LV004通信问题

Other Parts Discussed in Thread: DS90LV004
目前使用FPGA+DS90LV004通信,遇到通信不稳定的问题,希望得到大家的指导和帮助。
设计:设计原理图,FPGA+DS90LV004,三个通道作为发送,1个通道作为接收。测试时使用的通信线缆为工程级7类网线。
问题:
       1,芯片发热。不论是在FPGA没有烧写通信程序的情况下,也不论是FPGA运行通信程序的情况下,上电后,大约10秒后,用手摸就会感觉烫手。目前的PEM管脚都采用10K的上拉。
       2,通信不稳定。
               测试情况1:使用一块板子的两个接口,比如接口1的1脚和2脚最为发送端,与接口3的7脚和8脚作为接收端。400Mbps的频率下,可以发送和接收正常。:
               测试情况2:若使用两个板卡通信,两个板子的GND为同一个GND,比如,板卡1的接口1的1脚和2脚最为发送端,板卡2的接口3的7脚和8脚作为接收端。这时候通信就会不稳定(表现为:接收时钟频率正确,接收数据同步以后,会出现数据的高低位不断的串)。
              这两个测试情况,只是将通信的接口更换为了2个板卡的接口,就通信不正常了。而且使用示波器观察这两种情况的接收端信号,也没有明显差别。这是什么原因呢?如何解决?
      3,感觉有信号串扰:
             比如:板卡的接口1的1脚和2脚最为发送端,与接口3的7脚和8脚作为接收端,使用网线连接板卡的接口1和接口3。接口3可以接收到接口1发送的正常数据,而接口1的7&8脚也可以接收到一定的数据,数据存在错误。使用示波器观察,接口1 的7&8脚,也可以观察到数据波形。