This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

913 914 STP模式易挂掉,请教优化方法

Hi TI大大们好,

我们使用913+914方案,STP模式,Sensor是IMX323,Sensor晶振37.125MHz,通讯已正常,STP线已做屏蔽+双绞,主板端为2.54间距wafer连接器,Sensor端是1.0间距Wafer连接器,静止放置长时间运行正常。

但拿起晃动中间线缆或者触碰PCB,就容易数据丢失,图像卡住,VIN丢失。

开始觉得是接触不好,所以将两端的端子都使用UV胶固定,保证晃动时端子不晃动,测试效果稍微好一些,但仍然会发生,目前一直没有彻底的解决。

我们在软件上检测914的0x1C状态寄存器,以应对这种通讯异常,重新启动主控端的Sensor数据接收,但这终究还是没有彻底解决,用户体验很差。

所以发帖求助一下,STP模式下,我们应该怎样接线会更可靠,两边端子通常使用什么的连接器,PCB上应该如何处理能更抗干扰一些。

恳请赐教,谢谢。

附件  913  914的原理图

  • 您好,问题应该不是出在connetor上,应该是cable不符合要求,建议cable的回波损耗小于-10dB。 请参考这篇应用手册关于如何进行cable selection的介绍,其中return loss部分介绍了它是会影响稳定性工作的:
    www.ti.com/.../snla229.pdf
  • Hi Kailyn,

    感谢回复。

    我查看了snla229.pdf文档,关于ReturnLoss   

    Return Loss is the loss of the signal power resulting from a discontinuity in the characteristic impedance of the transmission line, and is most commonly encountered at the interface of one portion of the transmission line and another – such as the connector to a cable or board.

    所以看样子貌似主板和线之间的连接很关键,看了官方的好多资料,包括开发板都是同轴电缆的连接方式,最佳阻抗推荐为50Ω,由于产品外观和体积上的限制,目前我们采用的传统的2.54 wafer连接器(主板端),1.0 wafer连接器(Sensor端),请教下其他客户有没有使用STP模式的,使用了何种连接器?STP模式推荐用什么连接器?STP线缆的阻抗也为50Ω吗?

    感谢。

  • 您好,是的,不论选用STP还是coax,都是选用差分阻抗100ohm,单端阻抗为50ohm的cable,避免信号在传输过程中发生反射造成信号不完整,从而影响传输。
    另外,如果选用STP cable的话,connector建议使用Rosenberger HSD Connector 。 在DS90UB913的EVM user's guide中有相应介绍。 参考EVM user's guide Page17:

    www.ti.com/.../snlu135b.pdf
  • Thanks a lot~~  O(∩_∩)O