This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM26C32芯片使能问题

Other Parts Discussed in Thread: AM26C32

The device can be configure using the G and G logic inputs to select receiver output. The high voltage or logic 1 on the G pin, allows the device to operate on an active-high and having a low voltage or logic 0 on the G enables active low operation. These are simply a way to configure the logic to match that of the receiving or transmitting controller or microprocessor.

最近在使用AM26C32,发现datasheet中对于使能脚的描述,感觉和下面真值表有些冲突。请帮忙解答

  • 您好,前后不矛盾,使能引脚G为高有效,也就是说,当G=H的时候,不论G/是什么电平,当VID ≥ VIT+的时候,输出为H。
    同样G=H,不论G/什么电平,VID ≤ VIT—的时候, 输出为L。 如果G=L, G/=H,那么输出为高阻抗。 芯片disable。
  • The high voltage or logic 1 on the G pin, allows the device to operate on an active-high and

    having a low voltage or logic 0 on the G enables active low operation.

    Datasheet中提到,引脚G为高电压或逻辑1时,器件工作在高电平有效;

    引脚/G为逻辑0或低电平时,器件工作在低电平有效。

    不知道是不是我理解有误,而且如果按照真值表所属,/G引脚没有任何功能,是不是很多余。

    谢谢

  • 之前回复的复制有问题,可以看下截图

  • 您好,G和G/正好是两个逻辑相反的电平,使用其中任意一个都使得器件有效,比如说G=H,那么/G是高低电平都无所谓,或者说/G=L时,G是高低电平也无所谓。 也就是说,使得器件有效的话,使用G或者/G都可以,G是高有效,/G是低有效。 二者并不矛盾。