This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2594杂散问题

Other Parts Discussed in Thread: LMX2594

问题:

单环PLL,参考频率200MHz,鉴相频率200MHz,输出频率4.7GHz,观察输出频率发现在载波两侧100MHz处存在杂散,且无论我如何修改鉴相频率,输出频率,电荷泵电流,调制器阶数都无法定位杂散原因并消除;

双环PLL,采用参考环的输出频率作为第二个环的参考频率。当参考频率为200MHz时,依旧存在上述问题,且做出上述解决尝试无法解决问题;当参考频率220MHz时,载波两侧100MHz处无杂散,但是在载波两侧110MHz处存在杂散且无法消除(同时测试过大于200MHz的很多参考频率发现在载波两侧参考频率一半处都会存在杂散);当参考频率为190MHz时,其载波两侧一般频率处无杂散,只是在190MHz处存在参考频率杂散(同时测试过小于200MHz的很多参考频率都是这个情况)。

以上问题全部建立在LMX2594寄存器配置正确(我检查了很多次),锁定检测通过,跳频正常的情况下。

我也做过很多假设与验证,参考频率确定,鉴相频率修改成功,程序中也未进行二分频,外围电路也没有分频。

请问各位工程师前辈们,当参考频率>=200MHz时,载波两侧参考频率一半频率处存在杂散;当参考频率<200MHz时,只存在参考杂散,其载波两侧参考频率一半处不存在杂散,这个问题可能是什么原因导致的呢?你们有遇到类似问题又如何解决的呢?欢迎看到的前辈们,帮忙提供个解决思路,困扰小弟好多天,万分感谢!