This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7821数字隔离器-直流信号传输出错

Other Parts Discussed in Thread: DS90LV049, ISO7821

目前设计中使用ISO7821作为LVDS隔离收发器件,另外使用DS90LV049作为单端与LVDS的信号转换。测试中发现,时钟信号通过单端转差分再经过隔离器输出正常,但是如果是直流电平,比如3.3V逻辑高电平,则不管TTL信号是 0还是1,ISO7821的输出时钟是逻辑高,即差分350mV左右。也就是说,如果是直流逻辑信号,隔离器件好像无法正确传输,但是查阅datasheet,该芯片的速率范围为0-100Mbps,应该是可以用于直流传输的,不知道为什么出现目前的现象,哪位高手帮忙解答下,谢谢