目前设计中使用ISO7821作为LVDS隔离收发器件,另外使用DS90LV049作为单端与LVDS的信号转换。测试中发现,时钟信号通过单端转差分再经过隔离器输出正常,但是如果是直流电平,比如3.3V逻辑高电平,则不管TTL信号是 0还是1,ISO7821的输出时钟是逻辑高,即差分350mV左右。也就是说,如果是直流逻辑信号,隔离器件好像无法正确传输,但是查阅datasheet,该芯片的速率范围为0-100Mbps,应该是可以用于直流传输的,不知道为什么出现目前的现象,哪位高手帮忙解答下,谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ISO7821不是LVDS隔离器吗?手册上也是隔离lvds差分信号啊
感觉是ISO7821可以隔离交流信号,无法隔离直流信号,和手册说明不一致。同一个通道,6.5M的LVDS时钟可以正常通过,但是直流信号无法正确输出