各位工程师:你们好,我司在有一个DFP的应用,客户要求呢12V通过TYPE-C连接器输入电源给主板系统供电,同时这个接口客户可能会接一个TYPE-C接口的扩展HUB,支持DC-IN加上USB3.0,我们选了TUSB320,看资料如果仅仅是作为DFP的应用好像只是需要用到CC脚,其他的功能都没用到,请帮忙查下我司这个线路是否OKTUSB320.pdf,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位工程师:你们好,我司在有一个DFP的应用,客户要求呢12V通过TYPE-C连接器输入电源给主板系统供电,同时这个接口客户可能会接一个TYPE-C接口的扩展HUB,支持DC-IN加上USB3.0,我们选了TUSB320,看资料如果仅仅是作为DFP的应用好像只是需要用到CC脚,其他的功能都没用到,请帮忙查下我司这个线路是否OKTUSB320.pdf,
感谢您的回复,这个资料有看过,但是实际的情况还是有点差异,麻烦帮忙check下图,谢谢!
好的 谢谢 我们这个USB属于一种比较特殊的用法,不可能做UFP的模式(主板靠这个接口给整个系统供电),USB的使用需要外插一个Type-C接口的BOX,里面会有一个DC模块,我们这个接口只需要提供准确的USB3.0的信号连接就好。