您好!
我司产品应用是HDMI输入给SN65DP159 然后给TMDS442 ,最后HDMI信号输出,给下一级的SN65DP159,依次往复不断级联,可是级联到25级左右时,HDMI信号便会出现误码?请问是SN65DP159 的ReTime功能应用在这个方案不行还是说有什么需要注意的地方?
SN65DP159 HDMI输入端口使用交流耦合采用
整体方案:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,您这种多级级联应用我需要再确认下,那么PC到显示器之间的长度是多少需要级联25片retimer?
您好,谢谢您的回复!
我们的应用不是单纯的PC到显示器级联的,是每一级的设备都有PC设备输入和显示器输出的,通过TMDS442控制信号输入输出一级一级的级联形成信号环路,我们目前最大项目是需要级联100多台设备的。每一级之间的距离不远的,通常只有2米。目前25台设备形成的环路信号是稳定可以的。