现在用fpga采用select io解码908的lvds视频,没有稳定的vs,hs,de,现在905发过来的视频采用最简单的白屏,fpga能正确解码RGB数据为全ff,现在就是没有稳定的行场。视频分辨率1024x768@60hz,时钟65m。麻烦提点意见谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
现在用fpga采用select io解码908的lvds视频,没有稳定的vs,hs,de,现在905发过来的视频采用最简单的白屏,fpga能正确解码RGB数据为全ff,现在就是没有稳定的行场。视频分辨率1024x768@60hz,时钟65m。麻烦提点意见谢谢。
您好,谢谢回复,908解码出来的行,场信号,用FPGA的selectio来采样都是乱的,没有规律,没有满足1024x768@60hz的VS(场信号),HS(行信号),DE(视频数据有效信号),在一帧中,正常情况下DE应该是1024个clock,hs有768个。但是解码出来得这个几个信号都是乱的,我们用907给908来进行视频编解码,可以正常输出视频。但是用905跟908配,就不能显示视频了,麻烦您给点意见,谢谢。
我们试了用不带滤波的方式,即cofig[1:0]=00,还是一样的,我们现在测试用的硬件上管脚来默认配置,不使用I2C,但是i2c也可以用软核来配。905的配置现在如下:config[1:0]=00,vodsel=1,RFB=0,只是硬件配置,也可以使用I2C来修改。908配置:LFMODE=0,MAPSEL=1,config[1:0]=01,VODSEL=0。这是硬件配置,也可以用I2C来修改。现在我们用905和906回还测试可以正常解码,但是用905给908还是不行,不知道问题出在什么地方?