This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB954 對接 DS90UB953 和 DS90UB933的LOCK 問題

Other Parts Discussed in Thread: DS90UB935-Q1, DS90UB953-Q1, DS90UB933-Q1

您好,

使用DS90UB954 分別對接 DS90UB953 和 DS90UB933時,

954的reg 0X58[2:0]設為110: 50 Mbps (default for DS90UB953-Q1 or DS90UB935-Q1 CSISynchronous back channel compatibility) 時,可以同時LOCK 953 和 933 。

954的reg 0X58[2:0]設為000: 2.5 Mbps (select for DS90UB933-Q1 or DS90UB913A-Q1compatibility) 時,只能LOCK 933,不能LOCK 953 。

請問,實際使用上是否一律將954的reg 0X58[2:0]設為110: 50 Mbps就可以同時LOCK 953 和 933  ,

或是這只是特例,接 953 reg 0X58[2:0]就要設110: 50 Mbps,接 933 reg 0X58[2:0]就要設000: 2.5 Mbps ?

  • 您好,0X58[2:0]配置为110:50Mbps的时候,可以lock 953或者935。 而不是933. 

    0X58[2:0]配置为000:2.5Mbps的时候,可以lock 933或者913A。

    所以您前面配置为110:50Mbps的时候,写错了,不是同时lock 953和933哈,是953和935.

    因此,接953,需要配置为110, 接933, 需要配置为000, 不矛盾。 

  • 您好,

    我在實際使用時,當954的0X58[2:0]配置为110時,serializer端使用 953 或 935 或 933 或 913A 都是可以正常傳輸資料,

     所以才會詢問是否可以一律將0X58[2:0]配置为110,或是會有什麼隱患 ?

    謝謝