你好
我的需求是将MIPI CSI2信号传输距离从0.5m增加到5m,使用普通PCB+双绞线。
我在ti interface产品线中没找到专门针对MIPI信号的相关芯片,想请问一下使用DS25BR150 ,SN65LVDS20或者SN65DSI85是否可以满足需求?或者其他芯片?
谢谢!
Alan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
which one should I choose if the bitrate of my MIPI CSI2 has reached up to 1.4bps per lane ( approx 700MHz) ?