之前电路使用26MHZ有源晶振 配置输出可以锁定输出两路40.96MHz信号和一路32.768MHz
最近更改为40MHz有源晶振,但是配置锁定始终失败,参数从软件得到输入的
- 向咨询这个款芯片能否使用有源晶振做时钟输入 尤其40MHz ?配置选项应当选择LVCMOS clock Input 模式?
- 电路使用是否应当在晶振一侧并联51.1欧姆到底完成阻抗匹配?还是需要增加两个100欧姆上下拉1.8V?
- 这样配置数据有无问题?这样工作是否可以正常?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
之前电路使用26MHZ有源晶振 配置输出可以锁定输出两路40.96MHz信号和一路32.768MHz
最近更改为40MHz有源晶振,但是配置锁定始终失败,参数从软件得到输入的
crystal输入的话,输入频率不能超过32MHz,所以如果是40MHz输入,只能选择LVCMOS 输入。 因此需要符合LVCMOS 1.8V电平标准